Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What Are the Replacement Bus Plug Covers for the AP304G10 Busway?
Issue:
What Are the Replacement Bus Plug Covers for the AP304G10 Busway?

Product Line:
I-Line Busway and accessories sold and supported in the USA.

Environment:
Maintenance/Repair

Cause:
Selection

Resolution:
The part number is 45202-040-50. In addition, the  hinge spring pieces are required, two required per cover assembly.
Part # 45112-004-01,



Schneider Electric USA

Attachment(s)
BUSWAYDOORASSY.pdf [384.38 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings