Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: How does the HOM4RK2LA retaining kit install into the proper Homeline, single phase, 125 A max, convertible mains load center?
Issue:
Product Design Features

Product Line:
Homeline Load Centers

Resolution:
The HOM4RK2LA retaining kit secures one Homeline 2-pole branch circuit breaker to the Right side of the interior when used as a Back-Fed Main Breaker.
This retaining kit can ONLY be used for the Homeline, 100-125amp, Convertible main load centers, Series S01 and S02 and Plug-On Neutral Series S04 load centers. .
The retaining bracket will mount over the face of the back-fed branch breaker and get secured using the single interior mounting screw included with the kit.
NOTE: HOM-GFI and HOM-AFI branch circuit breakers are NOT suitable for use as back-fed main circuit breakers.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Make sure to obtain the correct 2-pole, Homeline branch breaker to be used as the back-fed Main and DO NOT exceed the maximum rating marked on each load center.
3) As shown in step 2, on page 2 of the intructions, remove and discard the interior mounting screw from the base (see Figure 1 for location)
4) Install the appropriate  Homeline back-fed branch breaker ONLY in positions 2-4 (The first two positions in the upper right side of the interior)
5) Center the retaining bracket over the breaker to be used as the back-fed breaker and press down against the face of the retaining bracket to seal it against the back-fed breaker.
6) Secure the retaining bracket to the base with the new interior mounting screw provided in the kit and torque to 35 lb-in (4 N-m)
7) Remove the backing of the wiring diagram label that comes in the kit, to expose the adhesive and attach the label to the inside of the load center enclosure or to the back of the cover.

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
HOM4RK2LA instructions.pdf [148.47 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings