Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the weathershield for a EX15T6H transformer?
Issue:
What is the part number for the weathershield for a EX15T6H transformer?

Product Line:
General Dry Type 600 Volts and Below

Environment:
Energy Efficient,  Three Phase Transformers, 18K enclosures, weathershield.

Cause:
Wants to make transformer NEMA 3R rated for outdoors.

Resolution:
The EX15T6H has a 17K enclosure which will take the 7400WS17K weathershield.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings