Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for AP406 Busway ?
Issue:
How to replace a section of AP406 Busway ?

Product Line:
Pre I-Line I Busway

Environment:
Maintenance

Cause:
Replacement

Resolution:
Replacement is a 100% neutral rated AP50610 Busway. The AP406 Busway was 4 wire , with only a 50% rated neutral. The new AP50610 will connect to existing with no other mounting adapters or accessories needed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings