Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the wire bending space for the Main Service Wires of a 200amp, QO or Homeline Load center?

Issue:
Product Design Features

Product Line:
QO and Homeline Load Centers

Environment:
Mains Wire bending space

Cause:
Information or application

Resolution:
The wire bending space is determine from the UL standards and the NEC, based on the mains amperage rating and maximum wire size the load center will accept. SEE THE NEC wire bending tables.

ALL the 200amp QO(Single and 3phase) and Homeline Main Breaker and Main Lug Load Centers meet the appropriate wire bending space requirements Per UL and NEC.

The 200amp QO(Single phase ONLY) and Homeline Main Breaker Load centers will have approximately 8.50 to 8.625 inches from the Top endwall down to the top surface of the Main Breaker lug for a Main Breaker load center.

The 200amp QO(Single phase ONLY) and Homeline Main Lug Load Centers will have approximately 11.50 to 11.625 inches from the top endwall down to the top surface of the Main lugs will be more, due to the load center not having a main breaker in the mains position







Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings