Issue:
Nema 4/4X Stainless Steel Panelboard Enclosures Meet ASTMA240 Standards
Product Line:
Stainless Steel panelboard enclosures sold and supported North America
Environment:
Specifications
Cause:
Application
Resolution:
Our Nema 4X/4 stainless steel panelboard enclosures do meet ASTM A240.
Nema 4/4X Stainless Steel Panelboard Enclosures Meet ASTMA240 Standards
Product Line:
Stainless Steel panelboard enclosures sold and supported North America
Environment:
Specifications
Cause:
Application
Resolution:
Our Nema 4X/4 stainless steel panelboard enclosures do meet ASTM A240.
Released for: Schneider Electric USA