Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do we have restrictions or recommendations for installing our motor control centers (MCC's) in seismic areas regarding flexible connections and lateral bracing requirements?

Issue:
Does a flexible connection satisfy the lateral bracing requirement for Motor Control Centers (MCC)?

Product Line:
Motor Control Centers

Environment:
Products sold and used in North America

Cause:
Equipment seismic qualifications

Resolution:
Please refer to page 24 and 25 of the MCC Installation, 80459-641-01E

"The structural civil engineer or design engineer of record is responsible for detailing the equipment connection and anchorage requirements (including the lateral restraint system if appropriate) for the given installation. The installer and manufacturers of the anchorage and lateral restraint system are responsible for ensuring that the mounting requirements are met. Schneider Electric is not responsible for the specification and performance of these systems.

​Each section must be anchored per detail supplied by the engineer of record to the load-bearing path of the building structural system."

Schneider Electric USA

Attachment(s)
page 24 and 25 80459-641-01E.pdf [783.42 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings