Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What size breaker is required for the SSP05EMA24, surge protective device
Issue:
What size breaker is required for the SSP05EMA24 Surge protective device?
Product Line:
Surge Protection Device

Environment:
Selectioon/application

Cause:
Installation

Resolution:
The EMA terminals accept a range of 10 AWG (6 mm2) to 2 AWG (34 mm2) copper wire for phase, neutral, and ground connectors.
We recommend a 30 A breaker for installation of these SPD's using #10 wire.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings