Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum AIC rating on through feed lugs in an NF panelboard:
Issue:
Maximum AIC rating on feed through lugs in an NF panelboard

Product Line:
NF panelboards and accessories sold and supported in North America

Cause:
Application/product selection

Resolution:
As a result of panel testing, feed through lugs on NF panels are limited to 25K per our design specifications.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings