Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the Masterpact breakers in PZ4 Switchgear 100% rated ?
Issue:
Are the Masterpact breakers in PZ4 Switchgear 100% rated ?

Product Line:
Power Zone 4 Switchgear

Environment:
Application

Cause:
Product features

Resolution:
Per Catalog 6037CT9901R4/05, page 38, it states, " Power-Zone 4 switchgear is industrial-duty equipment built to ANSI standards and uses 100% rated
Masterpact NW and NT circuit breakers"
See Catalog attachment below

Schneider Electric USA

Attachment(s)
PZ 4 6037CT9901.pdf [2.57 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings