Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the Square D lug part number for ILSCO number PB4-750-2N used in an I line Panelboard
Issue:
What is the Square D lug part number for ILSCO number PB4-750-2N used in an I line Panelboard ?

Product Line:
Panelboard

Environment:
Replacement

Cause:
Cross reference

Resolution:
The ILSCO lug part number PB4-750-2N, is the Standard Lug for Main Lug I Line Panelboard interiors. Square D's equal to ILSCO's number is 25098-25110 and it is rated for (4) 3/0 - 750 kcmil

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings