Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the Sub-feed circuit breaker mounting pan, in assembly NQSFB4Q?
Issue:
What is the mounting pan only from assembly NQSFB4Q?

Product Line:
NQ Panelboard Accessories

Environment:
Maintenance

Cause:
Replacement

Resolution:
If the mounting hardware is available, the part number for the Mounting Pan only is 80122-396-50. It is a non System recognized part for quoting and will need to be ordered onto the Plant with Line Code 8211.
If mounting hardware is also needed, (usually the case), an entire new Sub feed breaker kit, NQSFB4Q, will need to be ordered.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings