Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Size 00 Nema starters available in Nema 4X enclosures?
Issue:
Checking if size 00 Nema starters are available in Nema 4X stainless steel enclosures

Product Line:
NEMA Contactors and Starters

Environment:
NEMA 8502 and 8536 Type S Contactors and Starters

Resolution:
No, customer must select and use Size 0 for Nema 4X stainless steel.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings