Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: How does the PKSB1QOBF service barrier install into the low amperage, QO, fixed main lug, single phase load centers?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO Load Centers

Resolution:
The PKSB1QOBF Service Barrier is used ONLY with the QO load centers, Series 00_, (QO612L..,QO816L..and QO148L.) Fixed Main Lug single phase load centers when a branch breaker is used as a Back-Fed Main Breaker.
The Kit will contain 1 Service Barrier and 1 mounting screw
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.
Danger label
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Install the appropriate 2-pole, QO back-fed main breaker and DO NOT exceed the maximum amperage as marked on the load center wiring diagram.
3) Insert the service barrier tabs into the back-fed main breaker slots as shown in FIGURE 1 of the instructions.
4) Insert the mounting screw through the service barrier and into the load center base. Torque the screw to 25 lb-In(2.8 N-m). SEE FIGURE 1 of the instructions.
NOTE: It is easier to remove the complete interior base from the load center box, plug-on the back-fed main breaker, insert the service barrier, begin the threading of the screw, then re-install the interior base and continue to torque the service barrier mounting screw.
NOTE: The service barriers do not allow the load center to be serviced while energized. ALWAYS turn OFF all power to the load center before working on the load center.

NOTE: PLEASE MAKE SURE TO FOLLOW ALL THE INSTRUCTIONS THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings