Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where can I find the Data Bulletin 1640DB0702 for the comparison of the obsolete NQOD to new NQ panelboard ?

Article available in these languages: Spanish

Issue:
Assistance crossing the obsolete NQOD panels to the NQ and the comparison.

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
All the NQOD panels are obsolete.  The NQ panels are the replacement, however not a direct replacement. All components must be replaced.
For example, when replacing the NQOD424L100 you may consider the NQ418L1, MH26 box, NC26(F/S) mono-flat front or the MH26WP NEMA 3R enclosure.
Please refer to the attached Data Bulletin 1640DB0702 for the comparisons.

Schneider Electric USA

Attachment(s)
NQOD-NQ.pdf [135.73 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings