Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How is it possible to attach an I-line Welded Metal Directory frame in the field?
Issue:
How is it possible to attach an I-line Welded Metal Directory frame in the field? What are the part numbers for the Directory and what directory cards fit into it.?

Product Line:
I line Panelboard

Environment:
Application

Cause:
Installation

Resolution:
The Metal directory frame that is normally factory installed /welded, is part number 80114-161-01.   It is not self adhesive and most Installers attach these metal directory card holders in the field with a good epoxy adhesive like JB weld.   A Can of PK49SP Spray Paint will need to be ordered, since the directory frame is provided unpainted.
The Directory card that fits the metal holder is part number 80116-017-50

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings