Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the LJ suffix on an M or P frame breaker indicate?
Issue:
Define suffix LJ on an M or P frame breaker?

Product Line:
Circuit Breakers

Resolution:
The LJ suffix on an M frame or P frame breaker indicates that the breaker comes with lug kit AL800P7K factory installed. This gives the breaker a wire range of (2) 3/0 - 600 kcmil Al/Cu or (2) 3/0 - 750 kcmil compact aluminum only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings