Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do EX transformers come with a bottom cover?
Issue:
Are bottom cover plates provided with our EX transformers?

Product Line:
Transformers

Environment:
EX transformers

Cause:
Product features clarification

Resolution:
EX transformers that are rated 150KVA and below in the K style enclosures have bottom closing or cover plates. Transformers rated 225KVA
and above in the J style enclosures are switchboard construction, which means open bottoms.  There will not be any bottom plates or covers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings