Issue:
Older design repair parts
Product line:
EZM Metering
Environment:
Repair parts
Cause:
Maintenance
Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover - EZML332400C (includes labels)
Blank Covers - EZML400BK2 (Includes 3 Covers, these are the blank covers that go between the meter socket covers)
Cover Screws - 4020513002K (bag of 10 screws and the customer cover uses 12 screws)
Meter Socket Cover (cover for one meter position) - EZMCRC
Parts Kit - EZML3400KIT (This kit includes one complete meter position, meter socket line side through tenant breaker base)
Replacement Tenant Circuit Breaker (one per position) - LJL36400U31X
Circuit Breaker RB Cover - BCM (one position, this is the small plastic cover that goes over the tenant breaker handle)
Enclosure connecting hardware - 7329791750 (This bag contains 3 nuts, the installation instructions and the Series Combination System rated Caution Labels)
Mounting Channel - 7329776601 (This is the channel that gets mounted to the Wall or structure the EZM device will hang on)
Equipment Ground Bar Assembly - 7329704452 (Contains the 2 ground lugs mounted on the mounting bracket)
Mounting screws for Equipment Ground bar assembly - 2142217101 (2 required)
Branch load Neutral Lugs:
1) Lug kit - MMLK250 (This kit contains 3 lugs and mounting hardware, BUT the branch neutral will ONLY allow for 2 Lugs)
2) Lug Connector - 7329776906 (This is a flat bus bar the lugs mount on top of)
3) Mounting screws and washers for the Lug Connector - 2149020200(Screw for right side) & 2390331603(washer for right side) and 2159417320(Screw for Left Side) & 2390331201(Washer for Left Side)
End Closing Cap Kit - EZMCAP (Cap for covering Main Horizontal Cross Bus can be used on either Right or Left side)
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP (Cap for covering Main Horizontal Cross Bus on Right Side ONLY)
NOTE: (The closing caps ONLY come on the EZM Main Devices and should be relocated to the Ends of the EZM line up)
Older design repair parts
Product line:
EZM Metering
Environment:
Repair parts
Cause:
Maintenance
Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover - EZML332400C (includes labels)
Blank Covers - EZML400BK2 (Includes 3 Covers, these are the blank covers that go between the meter socket covers)
Cover Screws - 4020513002K (bag of 10 screws and the customer cover uses 12 screws)
Meter Socket Cover (cover for one meter position) - EZMCRC
Parts Kit - EZML3400KIT (This kit includes one complete meter position, meter socket line side through tenant breaker base)
Replacement Tenant Circuit Breaker (one per position) - LJL36400U31X
Circuit Breaker RB Cover - BCM (one position, this is the small plastic cover that goes over the tenant breaker handle)
Enclosure connecting hardware - 7329791750 (This bag contains 3 nuts, the installation instructions and the Series Combination System rated Caution Labels)
Mounting Channel - 7329776601 (This is the channel that gets mounted to the Wall or structure the EZM device will hang on)
Equipment Ground Bar Assembly - 7329704452 (Contains the 2 ground lugs mounted on the mounting bracket)
Mounting screws for Equipment Ground bar assembly - 2142217101 (2 required)
Branch load Neutral Lugs:
1) Lug kit - MMLK250 (This kit contains 3 lugs and mounting hardware, BUT the branch neutral will ONLY allow for 2 Lugs)
2) Lug Connector - 7329776906 (This is a flat bus bar the lugs mount on top of)
3) Mounting screws and washers for the Lug Connector - 2149020200(Screw for right side) & 2390331603(washer for right side) and 2159417320(Screw for Left Side) & 2390331201(Washer for Left Side)
End Closing Cap Kit - EZMCAP (Cap for covering Main Horizontal Cross Bus can be used on either Right or Left side)
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP (Cap for covering Main Horizontal Cross Bus on Right Side ONLY)
NOTE: (The closing caps ONLY come on the EZM Main Devices and should be relocated to the Ends of the EZM line up)
Released for: Schneider Electric USA