Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the analog meter ORICA5C in the legacy medical Panels?
Issue:
What is the replacement analog meter part number for the old medical meter ORICA5C?

Product Line:
Medical products remote indicator

Environment:
Replacement

Resolution:
The replacement is the current style  IG2000CBMPM. The LIM ( line isolation monitor) and connector plate will also need to be replaced. Select either the IG6KIT (which includeds IG6M (LIM) and the 4800IG6CBKTVM (connector plate and cables.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings