Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the standard primary and secondary lug kits for EE25S3H and EE25S3HCU?
Issue:
What are the part numbers for transformer lug kits, standard type for the single phase transformers  EE25S3H and EE25S3HCU?

Product Line:
Low voltage transformers

Environment:
EE25S3H and EE25S3HCU

Resolution:
The lugs listed below accept aluminum and copper wires.
For 480V primary use the DASKP100.
For 240V primary use the DASKP250.
For 120/240V sencondary use the DASKGS250.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings