Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you add 1 pole breakers to Medical Isolation panels?
Issue:
Why can't you add single pole breakers to medical isolation panels?

Product Line:
Medical Isolation Panels

Environment:
SIP, SID, SIX Medical Panels

Cause:
Application and Clarification

Resolution:
No. There is no neutral in medical Isolation panels. If you look at a typical secondary, there is only one coil.  It is floating in a magnetic field, but nowhere connected to ground.  The start is X2 and finish is X1.  A load connected between X1 and X2 will experience current flow across those two, at 120V.  Voltages from X1 or X2 to ground can read weird voltages, but only because they are reading floating voltages induced from electromagnetic energy circulating in the core.  That "phantom" voltage could be 60V, or it could be other voltages, depending on many factors. Adding a 1 pole circuit breaker will only be fed by half of the 120Vs required for the 120V circuit.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings