Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HOM2448L125PQGC, series S04, Homeline load center?
Issue:
Plug-On Neutral, Qwik-Grip design repair parts

Product Line:
Homeline Main Lug Load Centers

Resolution:
Only the parts listed below are considered field replaceable.
Cover - HOMC24UC (for optional white cover, HOMC24UCW)
Cover Mounting Screw - 4020513002K (bag of 10 screws)
Door Hinge - 4028356450K (contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Interior Assembly - HOM2448L125PQGCI (main lugs not included)
Main Lugs Kit - QOL125
Neutral Bonding Screw - 4028345850K
Equipment Ground Bar - PKGTALP2 (includes (1) PK9GTA and (1) PK18GTA with (1) LK100AN attached to the PK18GTA, which will leave 15 usable terminals on the PK18GTA)
Qwik Grip Endwall Inserts - PKQGI (one insert; each load center contains 4 inserts, 2 per endwall)
Qwik Grip bag assembly - PKQGA (contains 4 Qwik Grip shields that mount to the front of the inserts, 1 Qwik Grip diagram, 4 Qwik Grip filler plates, and an instruction bulletin)
Qwik Grip Fillers - PKQGFP (bag of 4)
Qwik Grip Shield - PKQGS (one shield; each insert requires a shield)

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings