Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What lugs are available for the Powerpact B frame breakers?
Issue:
What are the replacement mechanical and compression lugs for B frame breakers?

Product Line:
Circuit breaker, I-line Circuit breaker, Powerpact B frame, Unit-mount

Resolution:
I-Line B frame breakers ship with load end Al mechanical lugs as standard.
Unit mount circuit breakers are delivered with EverLink™ lugs on the line and load sides as standard.
Compression lugs are also available. Here are the part numbers and specifications for all of the field installable lugs:

Everlink table

Mechanical lug table

Compression lug table

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings