Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do QO or Homeline, NEMA 1(indoor) Type load centers have any hub provisions and if so what type of hub would they use?
Issue:
Product Design Feature

Product Line:
Homeline and QO Load Centers

Environment:
Hub Types

Cause:
Application

Resolution:
NEMA 1 load centers do not contain hub provisions, because they are ONLY indoor type load centers and cannot be used outdoors in a NEMA 3R application. Therefore, hubs are not required.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings