Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of breakers do the SIP, SID, SIX medical isolation panels use?
Issue:
What breakers are used on SIP, SID, SIX medical isolation panels?

Product Line:
Medical panels

Environment:
Class 4800 SID, SIP, and SIX

Resolution:
The QO and QOB breakers are used depending if the panel is for plug on or bolt on breakers. QO and QOB can both be used with the bolt on interiors.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings