Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the Class 9001 Type K, SK or KX operators be used in an area classified as Class 1 Division 1 hazardous locations?
Issue:
Is there a pushbutton that can be used in an area classified as Class 1 Division 1 & 2 hazardous locations?

Product Line:
Push Buttons and Operator Interface

Environment:
Type K, SK and KX

Answer:
The 9001 K SK KX are not rated for Class I Div 1.  Utilize the 9001BR product line stations OR an intrinsically safe system in Class I Div 1 applications.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings