Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
If a Masterpact breaker has a 100 A or 250 A sensor plug, can that sensor plug be replaced with a higher amp rating sensor plug?
Issue:
What is the maximum amp sensor plug that can be installed in a Masterpact breaker with 100 A or 250 A sensor plug?

Product Line:
Circuit Breakers

Resolution:
In a Masterpact breaker with a 100 A sensor plug, it is ok to change the sensor plug to 250 A, but not higher than 250 A.
In a Masterpact breaker with a 250 A sensor plug, it is ok to change to sensor plug to 100 A, but not higher than 250 A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings