Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the available padlock attachments for a QO, 2 pole, arc fault (CAFI) breaker?
Issue:
Can the QO220CAFI be locked on the ON or OFF position

Product Line:
Circuit Breaker

Resolution:
Two pole QO-CAFI breakers can be locked in the OFF position only using accessory QOGFI2PAF.
Two pole QO-CAFI breakers can be locked in either the ON or OFF position using accessory GFI2PA.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings