Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are any combination service entrance devices (CSEDs) with 225 A max bus rating available?
Issue:
Product Design Features

Product Line:
Combination Service Entrance Device

Resolution:
CSED = Combination Service Entrance Device
PoN = Plug On Neutral Interior


There are several ring type Homeline, 'Solar Ready' PoN, CSED's that contain 225 A max bus rating. Below are the catalog numbers of these devices.
Also, attached is a letter of certification for some additional catalog numbers and for some that did not reflect the 225A Max bus rating on the wiring diagram when the devices were first manufactured.
NOTE: There are NO other Catalog Numbers that contain 225amp Max. bus rating, unless the wiring diagram specifically states 225 A Max Bus Rating.

** Semiflush Mount Only
SC816F200PF
SC2040M125PF
SC2040M200PF
SC3042M200PF
SC3042M225PF

** Surface Mount Only
SC816F150PS
SC816F200PS
SC2040M200PS
SC3042M200PS
SC42M200PS

Schneider Electric USA

Attachment(s)
225 Amp Bus Rating Letter Of Certification.pdf [56.26 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings