Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How are 800A and above, PTQ style busway plug in units bolted to current style busway?
Issue:
How do you connect 800A, 1000A, or 1200A  PTQ type busway units to I-line II busway?

Product Line:
Busway

Environment:
AP and CP I-line II busway

Resolution:
The 800A and larger fusible plug-in units have catalog numbers beginning  with "PTQ" and utilize a bolted connection to the busway, requiring the removal of the plug-in base on the busway to make the connection. Once the plug in base adapter is removed they can bolt the switch unit to the busway.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings