Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the OSP sticker need to be ordered separately for SIP,SID,SIX medical panels? This is required by OSHPOD.
Issue:
Dose the medical panels like the SIP, SID, and SIX come with the OSP sticker required by OSHPOD?

Product Line:
Medical Isolation panel

Environment:
SID, SIP, and SIX

Resolution:
No. The OSP / Sesimic sticker is only included and available on Hospital or Medical Isolation Panels that have the NQ bolt on the interior. This would exclude all Controlled panels and any panel with QO load centers that accept only plug-on breakers. If they have any of these two panels and require the label, they will have to replace the panel with one with the NQ bolt-on interior. Replacement labels are not available.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings