Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where is the termination block for the X-ray panel, SXRM8A2F, door switch and LED located on the Medical Isolation SIP panel?
Issue:
How does the SXRM8A2F  Xray panel terminate to the standard SIP medical isolation panel?

Product Line:
medical isolation panel and X-ray panel

Environment:
SIP
SID
SIX
SXR

Resolution:
There is not a terminal block in the standard isolation panels. The SXRM8A2F can be used for the circuit but, they cannot use the door switch or the in use light. The switch and light are designed for the controlled medical isolation panel which is PLC controlled.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings