Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What ambient conditions are acceptable for operation and storage of Powerpact B frame circuit breakers?
Issue:
What is the range of the ambient temperature where a Powerpact B frame breaker can be put into service?

Product Line:
Molded Case Circuit Breakers

Resolution:
PowerPact B-frame circuit breakers may be used between -25°C (-13°F) and 70°C(158°F).
For temperatures higher than 40°C (104°F) inside the enclosure, devices must be derated. See table below as reference.

The permissible storage temperature range for PowerPact B-frame circuit breakers in the original packaging is -50°C (-67°F) and 85°C (185°F).
For more information you can check catalog 0611CT1603

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings