Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the CU400L61K3 lug kit be used with a 600AF/400AT LJA36400UXXX breaker, using (1) 600kcmil wire per phase?
Issue:
Will it be possible to terminate (1) 600kcmil wire per phase cable using the CU400L61K3 lug kit with a 600AF/400AT  LJA36400UXXX breaker ?

Product Line:
I line Breaker

Environment:
Application

Cause:
Installation

Resolution:
The CU400L61K3 lug kit is rated for (1) 3/0-600 kcmil / per phase Copper wire ONLY. For 600kcmil Copper wire, used in Raceway, the rating is 420A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings