Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for a transformer rated 250VA, 277 - 120V with fusing?
Issue:
What is the part number for a fusible control power transformer (CPT) rated 250VA, with  277V primary - 120V secondary?

Product Line:
control power transformer

Environment:
Class 9070TF

Resolution:
For a 250VA transformer rated 277V - 120V with fusing we suggest the 9070TF250D4. The primary fuse size is 2 - 2.5A and the secondary is 3A. The transformer accepts class cc fuses.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings