Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the end caps for the old I-line I busway?
Issue:
Part number for the end closing plates for old I-line busway.

Product Line:
Busway

Environment:
I-line busway

Cause:
N/A

Resolution:
In order to determine the correct end cap, you will need the complete part number, ampere rating, copper or aluminum, and plug in or feeder busway. Please see the attachment with the old items. Once you have selected the part number, pricing will need to be obtained from the local sales office and the lead time is 40 days.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings