Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is a vertical wall support for I-Line II busway when mounted in the vertical position?
Issue:
Vertical wall support for I-Line II busway when mounted in the vertical position.

Product Line:
I-Line II busway

Environment:
Installation/mounting

Cause:
N/A

Resolution:
Schneider Electric does not offer a vertical wall support busway hanger. We offer our standard vertical hangers, both fixed and spring types that the installer connects to
the wall using structural materials such as channel iron, square post, Kindorf, Unistrut, etc.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings