Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum available circuits, for a NQ panel rated120/240V 3 phase 4 wire Delta high leg voltage system?
Issue:
How many circuits can be added in one NQ panel rated for a delta high leg system?

Product Line:
Panels

Environment:
NQ panels

Cause:
N/A

Resolution:
NQ panels rated for a 240V delta high leg system, are restricted to 72 circuits max. That is as long as there are no more than 5 - 70A and above breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings