Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the NC100H Multi 9 supplementary protectors?
Issue:
Replacement breakers for the UL 1077 rated NC100H supplementary protectors

Product Line:
Circuit Breakers

Resolution:
The UL1077 listed C60SP devices are suitable replacements for the NC100H supplementary protectors.  The height and depth of the C60SP is identical to the NC100H. However, the width per pole is only 18 mm as opposed to the NC100H's 27 mm.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings