Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the heavy duty receptacle switches available in a NEMA 4X fiberglass enclosure?
Issue:
Selection

Product Line:
Heavy Duty Safety Switches

Resolution:
No. The Appleton Powertite and Crouse-Hinds Arktite switches are only available in NEMA 1, NEMA 4/4X/5 stainless steel, and NEMA 12/3R. The Hubbellock receptacle switch is available in NEMA 1 and NEMA 12 enclosures only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings