Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the Column width Panels have lockable doors ?
Issue:
What is the lock and key for a Column width NQ Panelboard ?

Product Line:
NQ Column Width Panelboards

Environment:
Application

Cause:
Product features

Resolution:
All Column Panels width trims and doors are lockable with the PK22FL lock and LP9618 keys, which are installed as standard construction.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings