Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement valve for VB-7263-203-6-7?
Issue:
Replacement valve for VB-7263-203-6-7

Product Line:
HVAC / Field Devices

Environment:
Valves

Cause:
Replacement / Installation / Maintenance

Resolution:
Replacement is VB-7263-0-4-07, the (-6)  in the old part number "VB-7263-203(-6)-7" indicates a special O-Ring that an OEM Dri-Steem uses.
The O-Ring has now been replaced and is indicated in the (-4) in the new Valve part number VB-7263-203-4-07. Also will need Linkage Kit AV-7400 to be used with the MK-2690 Actuator

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings