Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the GSA stand for on an I-line II busway plug in unit?
Issue:
What does GSA stand for or GSL stand for on busway units?

Product Line:
Busway

Environment:
I-line II

Cause:
N/A

Resolution:
GS = Gasket (Gasket material added to the interior perimeter of the door and added to the throat on the back of the plug-in unit)
A = Copper Compression Lugs (Factory installed copper compression lugs instead of the standard alumunim mechanical lugs) 600A units or less.
L = Copper Compression Lugs (Factory installed copper compression lugs instead of the standard aluminum mechanical lugs) 800A units or greater.

Please contact your local distributor or local Schneider sales office (if you are a distributor) for pricing as these are custom part numbers and not system recognized.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings