Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What's the difference between 118T145HDIT and 118T1659HDIT?
Issue:
Is there a difference between transformers 118T145HDIT and 118T1659HDIT?

Product Line:
Low Voltage Dry Type Transformers

Environment:
Application

Cause:
Product Features

Resolution:
The 118T145HDIT is a 460V Delta - 480/Y265V transformer , whereas the 118T1659HDIT transformer is a 460V Delta-460V Delta.
NOTE :
The 118T145HDIT with aWye secondary for drive isolation applications, is the more commonly used transformer.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings