Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What Main Circuit Breakers are used in the Series M02, EZM Mains Devices?
Issue:
Product Design Feature

ProductLine:
EZ METER-PAK Multi-Metering Equipment

Environment:
EZM Main Circuit Mreaker Main devices

Cause:
Application

Resolution:
EZ Meter-Pak Meter Center Circuit Breaker Mains are supplied with Factory installed Circuit Breakers ranging from 400A - 2000A, at 240 Vac Maximum, in 2-pole and 3-Pole configurations for use on following Systems:
120/240 Vac, 1-Phase, 3-Wire;
120/208 Vac, 1-Phase, 3-Wire (derived from a 3-Phase Network),
208Y/120 Vac, 3-Phase, 4-Wire
240/120 Vac, 3-Phase, 4-Wire DELTA.

EZM Mains with Circuit Breakers Rated 400A - 800A are of the Thermal-Magnetic Type consisting of the following:
EZM Mains Supplied with Lugs included:
Suitable for Underground or Overhead Feed
1-Phase                        Circuit                           3-Phase                        Circuit
Main Device                  Breaker                         Main Device                  Breaker
EZM1400CB LHP26400 EZM3400CB LHP32400
EZM1600CB MGP26600 EZM3600CB MGP36600
EZM1800CB MGP26800 EZM3800CB MGP36800

EZM Mains Supplied with NEMA Standard Lug Landing Pads included(Lugs to be purchased separately):
Configured for Underground Feed ONLY, and Meets EUSERC(West Cost Utility) Requirements
1-Phase                        Circuit                           3-Phase                        Circuit
Main Device                  Breaker                         Main Device                  Breaker
EZM1400CBU LHF26400 EZM3400CBU LHF36400
EZM1600CBU MGF26600 EZM3600CBU MGF36600
EZM1800CBU MGF26800 EZM3800CBU MGF36800

Thermal-Magnetic Circuit Breakers are supplied with Calibrated Fixed Thermal and Adjustable Magnetic Trip Functions.
The Magnetic Trip Function is adjusted by a single slider that simultaneously adjusts the Instantaneous trip point of each pole.
This Adjustable Instantaneous Trip Characteristic is Factory Set at the Minimum Setting allowing the Circuit Breaker to interrupt short circuit overcurrent with no intentional delay.
In a Motor Load Application this setting can be adjusted to allow for more inrush Current as the Motor reaches normal operating RPM.
For Multi-Family Residential Applications this Minimum Setting is typically the desired setting.

EZM Mains with Circuit Breakers Rated 1000A - 2000A are of the Electronic Trip Type consisting of the following:
EZM Mains Supplied with Lugs included:
Suitable for Underground or Overhead Feed (except as noted)
1-Phase                                Circuit                               3-Phase                                Circuit
Main Device                        Breaker                             Main Device                        Breaker
EZM11000CB PGP36100U31A (4) EZM31000CB PGP36100U31A (4)
EZM11200GCBT(1) PGM36120U31A(4) EZM31200GCBT(1) PGM36120U31A (4)
EZM11200JCBT (1) PJM36120U31A(4) EZM31200JCBT (1) PJM36120U31A (4)
EZM11200GCBU (2)(3) PGP36120U31A (4) EZM31200GCBU (2)(3) PGP36120U31A (4)
EZM11200JCBU (2)(3) PJP36120U31A (4) EZM31200JCBU (2)(3) PJP36120U31A (4)
EZM11600GCBC RGF36160U31A (4) EZM31600GCBC RGF36160U31A (4)
EZM11600JCBC RJF36160U31A (4) EZM31600JCBC RJF36160U31A (4)
EZM12000CB RJF26200 (5) EZM32000CB RJF36200 (5)
(1) Configured for Overhead Feed ONLY, not suitable for Underground Feed.
(2) Configured for Underground Feed ONLY, not suitable for Overhead Feed.
(3) Optional Lug Landing Pad Kit Available for Field Installation (Order Kit #: EZM1200ULL). SEE CAD DRAWING FOR OPTIONAL LUGS
(4) Breaker provided with Micrologic Standard 3.0 Trip Unit with adjustable LI Function (Adjustable Long-time, Adjustable Instantaneous). Trip Unit is interchangeable.
(5) 2000A Breaker supplied with Basic ET1.0I Trip Unit with Fixed Long Time, Adjustable Instantaneous Trip Function.  Trip Unit is NOT Interchangeable.

EZM Mains Supplied with NEMA Standard Lug Landing Pads included (Lugs to be purchased separately):
Configured for Underground Feed ONLY, and Meets EUSERC(West Coast Utility) Requirements (Except as Noted)
1-Phase                               Circuit                           3-Phase                              Circuit
Main Device                       Breaker                         Main Device                       Breaker
EZM11000CBU PGF36100U31A (6) EZM31000CBU PGF36100U31A (6)           .
EZM11200GCBE PGF36120U31A (6) EZM31200GCBE PGF36120U31A (6)
EZM11200JCBE PJF36120U31A (6) EZM31200JCBE PJF36120U31A (6)
EZM11600GCBU (8) RGF36160U31A (6) EZM31600GCBU (8) RGF36160U31A (6)
EZM11600JCBU (8) RJF36160U31A (6) EZM31600JCBU (8) RJF36160U31A (6)
EZM12000CBU (8) RJF26200 (7) EZM32000CBU (8) RJF36200 (7)
(6) Breaker provided with Micrologic Standard 3.0 Trip Unit with Adjustable LI Function, (Adjustable Long-Time, Adjustable Instantaneous) Trip Unit is Interchangeable.
(7) 2000A Breaker supplied with Basic Trip Unit ET1.0I with Fixed Long Time, Adjustable Instantaneous Trip Function.  Trip Function is NOT interchangeable.
(8) Does not meet EUSERC Requirements.

EZM Mains with Electronic Circuit Breakers are supplied with Trip Units designed for protection of Electrical Distribution Applications against over load currents.
Electronic Circuit Breakers also contain a Magnetic Trip Element in each pole with the Trip Point Adjustable from the front.


Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings