Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: How to install the 5th jaw kit (part number 5J) into a Meter-Pak and EZM branch device?
Issue:
Product Design Features

Product Line:
Meter Pak and EZM metering

Resolution:
The 5J fifth jaw kit is only for use on Square D meter sockets for network metering FROM a 208Y/120Vac system.
The below Square D Meter-Pak and EZM pre-fix catalog numbers can be used with this 5th jaw kit.

Meter Pak Prefix Devices:
- Ring Types - MP
- Ringless Types MPR and MPH
EZM Prefix Devices:
- Ring Type - EZM
- Ringless Type - EZMR and EZMH
SEE THE BELOW ATTACHED 5th JAW ASSEMBLY KIT INSERT CARD FOR KIT CONTENTS.
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.

Danger label
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
Once all Safety steps are followed, begin the 5J kit installation by following the instructions.
Make sure to install the 5th jaw kit on the correct Meter-Pak and EZM as shown in the instructions.
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
5J insert Card.pdf [85.07 KB]
Instructions for 5J kit.pdf [227.21 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings