Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the green covers for the PowerPacT B frames be ordered separately?
Issue:
Product Features

Product Line:
Molded Case Circuit Breakers

Resolution:
No, this cannot be ordered as a replaceable part. However, the green cover is not required, so there is no need to replace the breaker if just the green cover is damaged or missing.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings