Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QO154M200PQ, Series S06?
Issue:
Plug-On Neutral, Qwik-Grip, design repair parts

Product Line:
QO load centers

Resolution:
Only the parts listed below are considered field replaceable.
Load Center Cover - QOC54UF (flush cover would be used for both surface and flush applications)
White Load Center cover - QOC54UFW
Interior Assembly - QO154M200PQI (main breaker not included)
Neutral Bonding screw - 4028344850K
Main Breaker - QOM2200VH
Indoor Cover mounting screw - 4020513002K
Indoor Cover Hinge - 4028356450K (contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main circuit breaker and main lugs keps nut -2342702001
Ground bar Kit - PK23GTA
Qwik-Grip Fillers - PKQGFP (contains 4 fillers)
Qwik Grip Endwall Inserts - PKQGI (one insert; each load center contains 4 inserts, 2 per endwall)
Qwik Grip bag assembly - PKQGA (contains 4 Qwik Grip shields that mount to the front of the inserts, 1 Qwik Grip diagram, 4 Qwik Grip filler plates, and an instruction bulletin)
Qwik Grip Shield - PKQGS (one shield; each insert requires a shield)

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings