Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are HOMT quad tandem breakers available with (2) 2 pole circuits?
Issue:
Are Homeline tandem breakers available with (2) 2p circuits?

Product Line:
Circuit Breakers

Resolution:
Yes, HOMT tandem breakers are available with (2) 2p circuits, taking only 2 spaces in the panel.
  • The center poles are tied together and are common trip.
  • The outside poles are tied together and are common trip.
See the below table showing the catalog numbers as well as pictures.

Quad tandem table

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings